Case Study ® ABB 2025
Red Sea Project Company
Buildings
Residential
ABB powers Red Sea tourism project with smart energy technology
Saudi Arabia
Challenge
Spanning 28,000 square kilometers, the project is one of the world’s most ambitious regenerative tourism projects and will bring together the natural world with first class personalized accommodation, across an archipelago of more than 90 islands. 
Solution
The installation includes 10 System pro E power Low Voltage synchronization panels, rated 2500 up to 6300 Amps, which will generate 36MW power out of the 69 generators that will be installed at the Red Sea site. This use of smart low voltage synchronization panels will be supported by ABB Ability™ Energy and Asset Manager, a state-of-the-art cloud solution that integrates energy and asset management in a single intuitive dashboard.
Outcome
By monitoring data and taking corrective actions, the solution can reduce unplanned downtime to ensure continuous power supply and save up to 45 percent on operating expenses.